Full-filled Config (Uplink)
Bandwidth
Choices:
Downlink: Based on the Table 5.3.2-1 and 5.3.2-2 in 38.104
Uplink: Based on the Table 5.3.2-1 in 38.101-1 and 38.101-2
Select the Bandwidth configuration for the carrier.
Numerology
Choices: u = 0: 15 kHz | u = 1: 30 kHz | u = 2: 60 kHz Normal CP | u = 2: 60 kHz Extended CP | u = 3: 120 kHz
Select the numerology to be configured for current carrier.
Duplex Type
Choices: TDD | FDD
Selects the duplex type.
When TDD is selected, several TDD parameters appear below. These TDD parameters are reset to default values whenever numerology changes or FR changes. (The default values are different for each numerology.)
Transmission Periodicity
Sets the periodicity of DL-UL pattern. The choices are related to numerology.
Number of Downlink Slots
Sets the number of consecutive full DL slots at the beginning of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Number of Downlink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive DL symbols in the beginning of the slot following the last full DL slot.
Number of Uplink Slots
Sets the number of consecutive full UL slots at the end of each DL-UL pattern. The range is related to the numerology and slot configuration period.
Number of Uplink Symbols
Range: 0 ~ 14 for Normal CP; 0 ~ 12 for Extended CP
Sets the number of consecutive UL symbols in the end of the slot preceding the first full UL slot.
Number of Special Slots
Displays the number of special slots.
TDD Slot Allocation
Displays the TDD slot allocation for one period.
OFDM Type
Choices: DFT-s-OFDM | CP-OFDM
Select the OFDM Type for uplink.
Modulation
Choices: pi/2 BPSK | QPSK | 16QAM | 64QAM | 256QAM for uplink carrier; QPSK | 16QAM | 64QAM | 256QAM for downlink carrier
Select the Modulation type to be configured for current carrier.
RB Number Restriction
Choices: On | Off
Default: On
Enable or disable the RB number restriction when transform precoding enabled. If it is On, the UL-SCH RB number is restricted to (2^a * 3^b * 5^c) or less than BWP number. (a,b,c is non-negative integer).